Average Output Computation - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

In the case of binary types of input references, if the majority of inputs are at State 1 or the inputs are evenly split between State 1 and State 0, the Average output is commanded to State 1. If the majority of inputs are at State 0, the Average output is commanded to State 0.