IP Field Controller Hardware Tab - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

Attributes associated with the hardware source for object data are shown under the Hardware tab of the display panel. Attributes marked with the letter C are configurable and attributes marked with the letter W are writeable.

Table 1. IP Field Controller Hardware Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Computer Name

W

   

Contains the host name of the device.

Controller Number

C,W

0

Range = 000–999

Contains the three rotary switches that identify the device within the various levels of your site. Each rotary switch is selectable from 0 to 9, producing a number ranging from 000 to 999.

DHCP Enabled

C,W

True

False

True

Specifies whether a unique IP address is assigned automatically (True) or manually (False). A unique IP address is assigned automatically by the DHCP server or manually by the user.

Disable Automatic Alarming

C,W

False

False

True

Specifies whether automatic online/offline device event reporting is disabled (True) or enabled (False). This attribute only applies to the device and not to the device’s mapped objects. Devices with the Disable Automatic Alarming attribute set to True suppress the alarm event but still indicate they are offline in the navigation tree with a red X. Alarm extensions are not affected by this attribute.

Domain Name

W

   

Contains the network domain in which the device belongs to.

Ethernet MAC Address

W

00:00:00:00:00:00

 

Contains the unique hardware number that identifies the device within a network.

Instance Number

C,W

0

Range = 0–4,194,303

Contains the Object Instance part of the BACnet Object Identifier, which is used with the Object Type value to define the full BACnet Object Identifier value. The BACnet Object Identifier is used to establish communication with the object.

IP Mask

C,W

0.0.0.0

 

Contains the bit mask that defines which bits are used to separate between the host portion of the address and the domain portion of the address. The IP Mask consists of four numbers ranging from 0 to 255 separated by three periods.

IP Router Address

C,W

Listof[0]

 

Contains the address of the device which is used to forward messages to a remote IP network.

JCI IP Address

C,W

0.0.0.0

 

Contains the unique address other networks connected to the IP use to identify the device. The JCI IP address consists of four separate numbers ranging from 0 to 255 separated by three periods.