BACnet Hardware Tab - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

Attributes associated with the hardware source for object data are shown under the Hardware tab of the display panel. These attributes are not exposed to a BACnet network.

Note: Each Hardware attribute table is organized and divided into sections of Integration Hardware attributes, Device Hardware attributes, and Point Hardware attributes (calling out when attributes are shared between these object types). These sections are indicated by headings that span across the table. Attributes marked with the letter C are configurable and attributes marked with the letter W are writeable.
Table 1. BACnet Hardware Tab Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Disable Automatic Alarming

C,W

False

False

True

Specifies whether automatic online/offline device event reporting is disabled (True) or enabled (False). This attribute only applies to the device and not to the device’s mapped objects. Devices with the Disable Automatic Alarming attribute set to True suppress the alarm event but still indicate they are offline in the navigation tree with a red X. Alarm extensions are not affected by this attribute.

Instance Number

C

None

0–65,535

Remote Device Addr

 

None

BACnet device address

Remote Object Name

 

None