Object Deletion - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

Objects can be deleted offline in the system database on the SCT and later downloaded to the host device as part of the edited database. You can also delete objects with a browser if you have the Access Privileges to configure objects using the Security Administrator System. The user interface screens and procedures are similar in either case. Deleting an object involves selecting it in the Navigation Tree and using the Delete Items command.

See the Deleting Objects or Items section for more information.

Note: Before deleting an object, you should delete all references to the object within other objects and reconfigure any objects that are referenced in the object to be deleted. If the references are not edited or deleted, the referenced objects may not operate correctly. See the Engine Device Object for an example of how to locate incomplete references.