Object Creation - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

Objects can be created offline in the system database on the SCT and later downloaded to the host device as part of the edited database. You can also create objects with a browser if you have the Access Privileges to configure objects using the Security Administrator System. The user interface screens and procedures are similar in either case. Creating an object involves placing it at the desired position in the Navigation Tree and defining all the attributes that are required for it to operate. The procedure begins with the Insert Menu, and a wizard guides you through all the necessary configuration steps.

See the Creating Items with Wizards section for the steps to create objects/items.