BACnet Notes - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

The BACnet Notes column specifies if the attribute is exposed as a standard BACnet property and if it can be modified from a BACnet network.

Table 1. BACnet [System] Notes

Note

Definition

B - Exposed as Standard BACnet Property

Indicates that the attribute can be accessed as a standard BACnet Property of the equivalent BACnet Object Type from a BACnet network.

W - Writable

Indicates that the value of the attribute can be modified by a message from a device on the BACnet network.

Note: The types listed in Table 1 may also appear in the Note column, as applicable.