This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).
|
Attribute Name |
Notes |
Initial Value |
Values/Options/Range |
Description |
|---|---|---|---|---|
|
Enabled |
Indicates whether the Multiple Command object is enabled or disabled. |
|||
|
Executing |
False |
False, True |
Specifies the current execution status of the object. It is True when the object receives a state command and starts sending commands. When all actions are completed for a given state, this flag is set to False. |
|
|
Execution Priority |
C,W |
Indicates the relative importance of performing the function of the object within the device. |
||
|
Last Executed Date |
N |
Indicates the date stamp for the beginning of executing the current state. |
||
|
Last Executed Time |
N |
Indicates the time stamp for the beginning of executing the current state. |
||
|
Present Value |
D,W |
States Text attribute identifies the states set for this attribute. |
Indicates the current value of this object. |
|
|
Send OK |
Indicates the success or failure of the subordinate commands. If any subordinate commands failed, this attribute is set to False. When a send error is detected, a 5-minute timer is set. When the timer expires, the object is reevaluated and all commands are sent again. Commands may fail if the subordinate object is off-box and offline or if the subordinate object is set for local control. |
|
Attribute Name |
Notes |
Initial Value |
Values/Options/Range |
Description |
|---|---|---|---|---|
|
C,W |
Object Reference, Delay, Command ID, Parameters, Priority |
Lists actions to take for each supported state. Each action of the table contains a subordinate object reference, a delay, a command and its associated parameters, and a priority. The priority in this table is used only when Commands Priority is set to No Priority. The delay is the number of seconds before the given command is issued. Command delays can be lengthened or shortened to result in commands being sent out after, before, or at the same time as any other command. The total number of commands identified in the Action Table command set should not exceed 40. |
||
|
Command Priority |
C,W |
16 |
Uses Write Priority (Set 1). |
Determines the order by importance for all commands sent. If it is set to Priority None, commands will be sent at each individual priority specified in the Action Table attribute. |
|
Relinquish Default |
Specifies the default value to be used for the Present Value attribute when no commands are currently controlling this object. If this attribute is configured to any value other than None, the object sends commands for the value immediately. |