Meter Object - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

The Meter Object identifies the Metasys object (for example, Pulse Meter, AI, AV) that is used for the energy rate if the Demand Limiting strategy is configured. If only the Load Rolling strategy is used, a meter is not required.

The Meter Object should be defined on the same supervisory controller as the DLLR Object. Do not use an N1 Integration object for the meter unless you can guarantee that the NCM Service Time is always less than 60 seconds because the DLLR algorithm requires an updated meter value every minute.