LR Tariff Targets - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The LR Tariff Targets attribute lists the energy targets for the Load Rolling strategy. Each target consists of a target value and an entry from the Target Description set identifying the type of target, such as On-Peak. If the Load Rolling strategy is used, there must be at least one target defined. Only one target is active at a time. The Active LR Target attribute specifies which LR Target is currently active. The Target Description set includes:

  • Continuous

  • Off-Peak

  • On-Peak

  • Semi-Peak

  • Shoulder

  • Summer Off-Peak

  • Summer On-Peak

  • Winter Off-Peak

  • Winter On-Peak

  • Summer Semi-Peak

  • Winter Semi-Peak

  • Summer Shoulder

  • Winter Shoulder