Active LR Target - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The Active LR Target attribute specifies which of the defined Load Rolling targets is currently active. When this attribute changes, the Active LR Target Changed attribute indicates True until the start of the next interval if demand limiting is configured, or the next minute if load rolling only is configured. This attribute uses the Target Description enumeration set.