DL Tariff Targets - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

The DL Tariff Targets attribute is the list of energy targets for the Demand Limiting strategy. Each target consists of a target value and an entry from the Target Description set identifying the type of target, such as On-Peak. If the Demand Limiting strategy is used, there must be at least one target defined. Only one target is active at any time. The Active DL Target attribute specifies which target is currently active. The Target Description set includes:

  • Continuous

  • Off-Peak

  • On-Peak

  • Semi-Peak

  • Shoulder

  • Summer Off-Peak

  • Summer On-Peak

  • Winter Off-Peak

  • Winter On-Peak

  • Summer Semi-Peak

  • Winter Semi-Peak

  • Summer Shoulder

  • Winter Shoulder