Allow Reset in Shed Mode - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

The Allow Reset in Shed Mode attribute controls whether the Reset Initialization Parameters command can be issued while DLLR is in Shed mode. When True, the Reset Initialization Parameters command can be issued once if DLLR is in Shed mode. As soon as the command is issued, this attribute is automatically reset to False and must be manually set to True before the command can be issued again in Shed mode.