Active LR Target Changed - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

The Active LR Target Changed attribute displays True when the Active LR Target value is changed. It is set to False at the start of the next interval if demand limiting is configured, or at the start of the next minute if load rolling only is configured. This attribute allows the DLLR object to raise an alarm when the LR target changes.