Auto Shutdown Attributes - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

This object contains attributes common to many Metasys system objects. These additional common object attributes are described in the Common Object Attributes section.

Note: In the Notes column, letters indicate the following: C - Configurable, R - Affected by Extension’s Reliability, and W - Writable.
Table 1. Auto Shutdown Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Control

C

   

Determines, in conjunction with the Shutdown State, if an alarm shutdown should occur. This is the current state of the references control point.

Dependents

C,W

 

Number of Entries = 1–32

Uses each dependent object identified in this list of object references to locate the Alarm object that is to have its alarm reporting controlled by the control point.

Enabled

 

True

  Indicates whether the Auto Shutdown object is enabled (True) or disabled (False).

Execution Priority

C,W

Normal

  Indicates the relative importance of performing the function of the object within the device.

Present Value

R

Off

On = 1

Off = 0

 

Reliability

 

Input Unreliable

Various

Reflects the reliability of the control point. When the control point is not reliable, the Reliability attribute becomes Input Unreliable.

Shutdown State

C,W

 

Uses the value set of the control point once the Auto Shutdown object reads the control point value.

Determines the definition of the shutdown state. When the control point goes to the state defined as the shutdown state, Auto Shutdown disables alarms from the point.

Startup Delay

C,W

5

Units = Minutes

Represents the time in minutes that must elapse before alarm reporting is re-enabled, once the control point changes from the Shutdown State to any other state.

States Text

      Indicates the displayed strings for the Present Value.