Wireless Receiver Supervisor Object - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The Wireless Receiver Supervisor object is the root of the Wireless Sensor integration. The Wireless Sensor integration allows the NAE to communicate with the wireless sensing system over the Ethernet network. The Wireless sensing system consists of wireless receivers and wireless sensors.

Each integrated wireless field device (Wireless Receiver Object) and field point object (Wireless Sensor Object) appears under the Wireless Receiver Supervisor object in the Navigation Tree. Only one Wireless Receiver Supervisor object can be configured in each NAE or NIEx9.

Note: The Wireless Receiver Supervisor object is not available for network engines updated to Release 9.0.7 and later.