The following table lists the commands supported by the SA Bus Integration Object.
|
Command Name |
Parameters |
Description |
|---|---|---|
|
Activate Provisioning |
None |
Requests the SNC to provision the new firmware that is pending in its memory. This process activates the firmware. You can monitor the status of this action under the Progress column of the Provisioning tab. |
|
Clear Statistics |
None |
Clears the statistics for the integrated SA Bus. |
|
Latch Statistics |
None |
Updates the displayed SA Bus statistics with the current values. |
|
Refresh Provisioning Discovery |
None |
Refreshes the SA Bus Provisioning view on the SA Bus of the SNC. Send this command if an SA Bus device that is connected to the SNC is not showing up in the SA Bus Provisioning view. The command takes several minutes as the SNC searches for devices over its SA Bus. Found devices are added to the Provisioning view. For example, use this command to locate an IOM that is stuck in a boot-code-only mode because of some type of failed provisioning cycle. For most cases, the Refresh Provisioning Discovery command is rarely needed. |