Attribute commands are commands you can issue from the GIO to individual attributes of the GIO. To access the attribute commands, do one of the following:
-
In the navigation tree, right click on the GIO object and select Commands then select an attribute for the GIO Attribute Command, and click the ellipsis button.
-
In a category view for the GIO (in the display frame), right-click on the attribute you want to command, and select Commands.
The attribute commands that appear are based on the data type of the attribute and whether Override Allowed and Adjust Allowed are True or False. See Table 1 for more information about these elements.
| Command | Notes |
|---|---|
|
Adjust phq1586283815223.html#ciz1559299015970__fn_adjust_allow_must |
Real values only (floating points) |
|
Operator Override phq1586283815223.html#ciz1559299015970__fn_override_allow_must |
|
|
Release Operator Overridephq1586283815223.html#ciz1559299015970__fn_override_allow_must |
|
|
Change Units |
All values but True/False |
|
Change Name |
|
|
Change Display Precision |
Real values only (floating points) |
|
State0...StateNphq1586283815223.html#ciz1559299015970__fn_adjust_allow_must |
Two state or multistate values |
|
Truephq1586283815223.html#ciz1559299015970__fn_adjust_allow_must |
True/False only |
|
Falsephq1586283815223.html#ciz1559299015970__fn_adjust_allow_must |
True/False only |