BACnet IP Integration Object - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The BACnet IP Integration object manages the communication with a BACnet/IP network. All integrated BACnet devices and objects appear under the BACnet IP Integration object in the Navigation Tree.

The BACnet IP Integration object serves as the root for all integrated BACnet/IP Field Controller objects on an Ethernet trunk. The BACnet IP Integration object is a direct child of a supervisory controller and integrates BACnet/IP devices using the Ethernet trunk.

For general information on Metasys system objects, see the Object Help section.

For detailed information on the BACnet IP Integration object, see BACnet IP Integration Attributes.