About this task
Notes:
- This process is the same when the system is offline, except the binding is done to the archive database instead of the online system.
- For information on default preferences for graphics (such as status colors, fan colors, state colors, and alarm flashing settings), see Graphic Settings Tab in the Preferences section.
To create a complete graphic: