About this task
Use this procedure if you want to edit a background of a graphic by exporting it from the UGT. Use this method when a copy of the existing background image is not available.
Procedure
Results
Note: Save a copy of the background image file in a folder on your hard drive as a backup method. If
you decide to edit that background image later, you can edit your hard drive copy
and use the Set Background Image icon to re-import the
background into the graphic in the UGT. You also can use your hard drive copy in the
event that you lose your databases and need to recover the background image.