The User Graphics tool runs in either Edit Mode View Mode. When you are generating new graphics or editing graphics, the User Graphics tool is in Edit mode. When you finish editing and click save and the UGT switches to View mode.
You can generate graphics in the Metasys system with the online mode or with the offline mode:
Online: Use this method if your web browser is connected to an Engine or Metasys server . In this case, a new graphic is generated online in the device where the graphic resides during normal operation. When you are finished creating or editing graphics, Upload the database to the archive database in the SCT.
Offline: If your web browser is connected to the SCT. If this case, the new graphic is generated offline and stored in the archive database. When you are finished creating or editing graphics, Download the database to the device where the graphic resides during normal operation.