Monitoring and Commanding Items Using Graphics - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

About this task

Note: The Site Management Portal UI provides the capability to monitor and command the Metasys system from a graphic.

To monitor your Metasys system using graphics:

Procedure

  1. Open a graphic to display the current status/state of system components.
  2. Navigate through the system.
  3. To command Metasys objects or items using graphics, right-click the graphic element to open the User Actions Panel and click More Commands. Select from the available commands. To change the value of a Metasys object or item from an inline command box, click inside the box, type a new value, and press Enter. For information on the runtime behavior of a particular graphic element, refer to the Graphics+ Runtime Help (LIT-12011708).