|
Attribute |
Description |
|---|---|
|
Effective Period |
The Effective Period attribute defines the range of dates within which the Schedule object is active. By default, these dates are unspecified, causing the Schedule object to be active for all days. When the Schedule is not within the Effective Period, the Schedule is considered Inactive and the Schedule’s status is set to Inactive. Wildcard may be used in the date fields. |
|
Schedule Output Type |
Schedule Output Type Options
|
|
Default Schedule Command |
The Default Schedule Command attribute indicates the command of the Schedule object when no event is in effect, due to no scheduled command or a conscious gap in the schedule. The Default Schedule Command is executed every midnight unless another event is in place to begin at midnight. The Default Schedule Command also supports the Release command. The Release command releases the Scheduling function’s control of the scheduled objects. Setting the Default Schedule Command to Release is the only available method to release the schedule’s control of scheduled objects through the Schedule object. Release should only be used for the Schedule Default Command if the scheduled items support the Release command. |
|
States Text |
The States Text attribute indicates the displayed strings for the Present Value when the Schedule Output Type is either binary or multistate. This attribute allows you to change what states the Schedule’s Present Value displays if you want it to be different from the key item. |
|
Display Units |
The Display Units attribute indicates the displayed units of the Present Value when the Schedule Output Type is analog. This attribute allows you to change the units displayed with the Schedule’s Present Value if you want them to be different from the key item. |