|
Command Name |
Number of Parameters |
Description |
|---|---|---|
|
Disable |
None |
The Disable command stops all future scheduled events. Neither the Weekly Schedule nor the Exception Schedule run again until the Schedule object is re-enabled. While disabled, the status log in the Scheduled Items view lists the object as disabled. The schedule remains disabled until re-enabled. |
|
Enable |
None |
The Enable command allows the Schedule object to resume normal scheduling operation. The Schedule object starts the schedule as soon as it is enabled. When it is re-enabled, the Schedule object writes its current value to the scheduled items. |