Multistate Output Object - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

The Multistate Output object’s attributes represent the desired state of one or more physical outputs or processes of the device in which the object resides. The actual functions associated with a particular state are determined locally (not part of protocol). Present Value represents the state with a number, and State Text associates a description with each state.

The Multistate Output object integrates N1, N2, and BACnet controllers with supervisory controllers, resulting in:

  • a consistent interface to point objects for all controller types

  • flexibility in point mapping

  • support for Metasys controllers

For example, this object allows you to command the modes of an access control device from a supervisory controller.

Note: The N1 migration Multiple Command object maps to this Multistate Output object.

For general information on Metasys system objects, see Common Object Attributes.