Binary Input Commands - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The table below lists the commands supported by the Binary Input Object.

Table 1. Binary Input Commands

Command Name

Number of Parameters

Description

Disable Alarms

None

Enable Alarms

None

In Service

None

Note: For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.

Out of Service

The value to be written to the Present Value.

Note: For BACnet objects, support of this command is dependent on the ability to write the Out Of Service attribute.

Temporary Out of Service

The value to be written to the Present Value attribute, along with the hours and minutes that the out of service state is temporarily active.

Allows a user to temporarily override the object’s hardware input for simulation or other purposes for a specified period of time stated in hours and minutes. This command has the same function as an Out of Service command but with the time element.