Analog Value Commands - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The table below lists the commands supported by the Analog Value Object.

Table 1. Analog Value Object Commands

Command

Parameters

Description

Adjust

None

The value to be written to the Present Value attribute. The value must be less than Max Present value and greater than Min Present Value.

Disable Alarms

None

Enable Alarms

None

Operator Override

None

The value to be written to the Present Value attribute.

Release Operator Override

None

Release

None

Release All

None

Important:

The Release All command may not cause an immediate return to automatic operation. The Release All command clears all command priorities, including those that come from applications and features. When this happens, the output point goes to its Relinquish Default condition. In some cases, the application or feature may have sent a command that does not match Relinquish Default. In this instance, the output point does not end in the state that the applications or features intended. This situation can cause unexpected operation to occur; for example, a space could overcool or overheat, a fan might run longer than expected, and so on. Also, if an operator has overridden an input, use the Release Operator Override command.

Temporary Override

The value to be written to the Present Value attribute, in addition to the duration of the override in hours and minutes.

Overrides a point temporarily for a specified period of time. After the specified time period passes, the Override is automatically released.