Analog Input Commands - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

The table below lists the commands supported by the Analog Input Object.

Table 1. Analog Input Commands

Command Name

Parameters

Description

Disable Alarms

None

Enable Alarms

None

In Service

None

Note: For BACnet objects, this command is dependent on the ability to write the Out Of Service attribute of the BACnet Analog Input object in the remote BACnet device. Objects in the N30, for example, do not support this command.

Out of Service

The value to be written to the Present Value attribute.

Notes:

  • For BACnet objects, this command is dependent on the ability to write the Out Of Service attribute of the BACnet Analog Input object in the remote BACnet device. Objects in the N30, for example, do not support this command.
  • For integrated N2 objects, this command is dependent on the ability to set the AI point in the N2 controller to an override state. System 91 controllers, for example, do not support this command.

Temporary Out of Service

The value to be written to the Present Value attribute, along with the hours and minutes that the out of service state is temporarily active.