Menu Selection:
Inserts one of the following types of field points into a field device under an integration:
-
N2 Trunk
Analog Input Object (AI), Analog Output Object (AO), Accumulator Object, Binary Input Object (BI), Binary Output Object (BO), Multistate Input Object (MI), Multistate Output Object (MO)
-
BACnet
All field points listed for the N2 trunk plus Analog Value Object (AV), Averaging Extensions, Binary Value Object (BV), Calendar Object, Electric Demand Control Object, Electric Demand Monitoring Object, Event Enrollment Object, Generator Load Control Object, Group Object, Life Safety Point Object, Life Safety Zone Object, Multistate Value Object (MV), Notification Class Object, Schedule Object, Trend Log
-
IP Field Controller
Analog Input Object (AI), Analog Output Object (AO), Analog Value Object (AV), Accumulator Object, Binary Input Object (BI), Binary Output Object (BO), Binary Value Object (BV), Calendar Object, Multistate Value Object (MV), Notification Class Object, Schedule Object, Trend Log
-
MS/TP Field Bus Integration
Analog Input Object (AI), Analog Output Object (AO), Analog Value Object (AV), Accumulator Object, Binary Input Object (BI), Binary Output Object (BO), Binary Value Object (BV), Calendar Object, Multistate Value Object (MV), Notification Class Object, Schedule Object, Trend Log
-
LON Trunk
Analog Input Object (AI), Analog Output Object (AO), Accumulator Object, Binary Input Object (BI), Binary Output Object (BO), Multistate Input Object (MI), Multistate Output Object (MO), Generic Integration Object (GIO)
Note: You can no longer manually add a GIO to a LON trunk; however, the GIO is still supported in existing databases, even after upgrading to the next software release. -
N1 Migration
All field points listed for the N2 trunk plus Generic Integration Object (GIO) and N1 PID Loop Object.
-
VND Integration (Vendor)
Analog Input Object (AI), Analog Output Object (AO), Accumulator Object, Binary Input Object (BI), Binary Output Object (BO), Multistate Input Object (MI), Multistate Output Object (MO)
-
Wireless Supervisor Integration
-
XL5K (Excel 5000/XL-5000) Integration
See one of the following sections for more information: