BACnet Device Attributes - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Note: In the Notes column, attributes that are marked with a letter C are configurable, attributes marked with the letter W are writable, and attributes marked with the letter D indicate the default attribute for the display.
Table 1. BACnet Device Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Description

Alarm State

Indicates the current state of the object.

Align Intervals

W

False

Specifies whether clock-aligned periodic time synchronization is enabled. If periodic time synchronization is enabled and the time synchronization interval is a factor of an hour or a day (that is, the value divides without remainder), then the beginning of the period specified for time synchronization aligns to the hour or day, respectively.

APDU Retries

W

3

Indicates the maximum number of times that an Application Protocol Data Unit (APDU) is retransmitted. The default value is 3. If this device does not perform retries, then this attribute is zero. If the value of this attribute is greater than zero, a nonzero value is placed in the Device object APDU Timeout attribute.

APDU Segment Timeout

W

4,000

Indicates the amount of time in milliseconds between retransmissions of an APDU segment. This value is nonzero if APDU Retries is nonzero. The APDU Segment Timeout attribute is present if segmentation of any kind is supported.

In order to achieve reliable communication, the values of the APDU Segment Timeout attributes of the Device objects of all intercommunicating devices should contain the same value.

Note: If segmentation of any kind is supported, this attribute is required.

APDU Timeout

 

See next column

Indicates the amount of time in milliseconds between retransmissions of an APDU requiring acknowledgement for which no acknowledgement has been received. This value is nonzero if APDU Retries is nonzero.

In order to achieve reliable communication, the values of the APDU Timeout attributes of the Device objects of all intercommunicating devices should contain the same value.

The default is 6,000 milliseconds for devices that permit modification of this attribute. The default value is 60,000 milliseconds for all other devices.

Active COV Subscriptions

   
Contains a list of BACnet COV Subscriptions, each of which consists of a Recipient, a Monitored Property Reference, an Issue Confirmed Notifications flag, a Time Remaining value, and an optional COV Increment. This attribute provides a network-visible indication of those COV subscriptions active at any given time. Whenever a COV Subscription is created with the Subscribe COV or Subscribe COV Property service, a new entry is added to the Active COV Subscriptions list. Similarly, whenever a COV Subscription is terminated, the corresponding entry is removed from the Active COV Subscriptions list.
Note: If the device supports execution of either Subscribe COV or Subscribe COV Property service, this attribute is required.

Alarm State

   

Indicates the current status of the object. The expected state is Normal.

Appl SW Version

   

Identifies the version of the application software installed in the device. The content of this string is locally defined (date-and-time stamp, a programmer’s name, a host file version number, and so on).

Backup Fail Timeout 1

W

120

Indicates the number of seconds that the device being backed up or restored waits before unilaterally ending the backup or restore procedure. This attribute is writable (the device performing the backup, or the operator, configures this with an appropriate timeout).

Units = Seconds

Configuration Files

   

Identifies the files within the device that determine what device image can be backed up. The contents of this attribute are only required to be valid during the backup procedure. If the device supports the BACnet backup and restore procedure, this attribute is supported.

Note: If the device supports the backup and restore procedures, the Configuration Files and Last Restore Time attributes are required.

Database Revision

   

Specifies a logical revision number for the device’s database. Database Revision is incremented when an object is created or deleted, an object name changes, or a restore is performed.

Description

W

 

Contains a string of printable characters used to describe the application being run by the device or other descriptive information.

Unrestricted range.

Device Addr Binding

W

 

Contains a list of BACnet Object Identifiers of a BACnet Device object and a BACnet device address in the form of a BACnet Address. Entries in the list identify the actual device addresses that are used when accessing the remote device through a BACnet service request. The list may be empty if no device identifier-device address bindings are currently known to the device.

DST Status

W

  Indicates whether daylight saving time (DST) time is in effect (True) or not (False).

True, False

Graphic

C,W

  Indicates the graphic associated with the object.

Graphic Alias

C,W

 

Indicates a portion of the graphic’s item reference, up to and including the name of the folder containing this object or the controller containing this point. Maximum 256 characters

Interval Offset

C,W

0

Specifies the offset, in minutes, from the beginning of the period defined for time synchronization until the actual time synchronization requests are set. Interval Offset has no effect when Align Intervals is False. Units = Minutes

Last Restore Time

   

Specifies when the device’s image was last restored. If the device supports the BACnet backup and restore procedures, this attribute is supported.

Note: If the device supports the backup and restore procedures, the Configuration Files and Last Restore Time attributes are required.

List of Session Keys

   

Contains a list of the cryptographic keys used to communicate with other security-conscious BACnet Devices. This attribute is not readable or writable by any device except a device designated the Key Server. A session key consists of a 56-bit encryption key and a BACnet Address of the peer with which secure communications is requested.

Local Date

W

  Indicates the date. If the device has no knowledge of time or date, Local Date is omitted.

Local Time

W

  Indicates the time of day. If the device has no knowledge of time or date, Local Time is omitted.
Location

W

  Indicates the physical location of the device.

Manual Time Sync Type

C,W

Automatic

Configures the type of BACnet Time Synchronization to send to a BACnet device.
  • UTC: UTC time synchronization message is sent.
  • Local: A local time synchronization message is sent.
  • None: No message is sent.
  • Auto: The mapper object's Protocol Services Supported attribute is used to determine which type of time sync is supported, and if:
    • utcTimeSynchronization is set, the code functions as if Time Sync Type is set to UTC.
    • utcTimeSynchronization is not set and timeSynchronization is set, local time is set.
    • neither utcTimeSynchronization nor timeSynchronization is set, an error is returned.

Max APDU Length

   

Specifies the maximum number of octets contained in a single, indivisible application layer protocol unit. Underlying data link technology constrains the value of this attribute.

Greater or equal to 50

Max Info Frames

 

10 (FEC)

20 (NxE)

Specifies the maximum number of information frames the node may send before it passes the token. This attribute is present if the device is a node on an MS/TP network. If Max Info Frames is not writable or otherwise user configurable, its value is one.

Note: If the device is an MS/TP manager node, both the Max Info Frames and Max Manager attributes are required.

Max Manager

 

127

Specifies the highest possible address for manager nodes and is less than or equal to 127. This is present if the device is a manager node on an MS/TP network. If Max Master is not writable through BACnet services, its value is 127.

Note: If the device is an MS/TP manager node, both the Max Info Frames and Max Manager attributes are required.

Max Segments Accepted

    Indicates the maximum number of segments of an Application Protocol Data Unit (APDU) accepted by the device.

Model Name

    Contains a name assigned by the vendor to represent the model of the device.

Offline

 

False

Displays the offline or online status of connected hardware.

Profile Name

   

Contains a string of characters that represents the name of the object profile to which the object conforms. A profile name must begin with a vendor identifier code in base-10 integer format, followed by a dash. The vendor identifier code indicates the organization that administers the remaining characters of the profile name, and publishes and maintains the profile document identified by the profile name. The vendor identifier does not need to match the vendor identifier of the device in which the object resides.

Protocol Obj Support

   

Indicates which standardized object types the device’s protocol implementation supports. This attribute reflects the minimum set of object types, but implementation often supports additional standard and non-standard object types with their own set of attributes. (The list of attributes supported for a particular object may be acquired by use of the Read Property Multiple service with an attribute reference of All.)

Protocol Revision    

Indicates the minor revision level of the BACnet standard. This starts at 1 and increases for each subsequent release.

If the Protocol Version attribute changes, this number reverts to zero. This attribute is required for all devices with BACnet Protocol Version 1, Protocol Revision 1 and above. If this attribute is not present, the device is Protocol Version 1, Protocol Revision 0.

Protocol Ser Support

   

Indicates which standardized protocol services the device’s protocol implementation supports. This attribute reflects the minimum set of services, but implementation often supports additional standardized services.

Protocol Version

   

Represents the BACnet protocol the device supports. Initial releases are Version 1; subsequent releases increase the number by one.

Restart Notification Recipients

C,W

 

Controls the restrictions on which devices, if any, are notified when a restart occurs. The value of this attribute is a list of BACnet Recipients. When the length of this list is empty, the device cannot send a device restart notification. The default value of this property is a single entry representing a broadcast on the local network. If the list has one or more entry, the device sends a restart notification, but only to the devices or addresses listed.

Segmentation

   

Indicates if the BACnet device supports segmentation of messages. If so, it supports segmented transmission, reception, or both.

Segmented Both, Segmented Transmit, Segmented Receive, No Segmentation

System Status

D

  Reflects the current physical and logical state of the device.

Operational, Operational Read Only, Download Required, Download in Progress, Nonoperational, Backup in Progress

Time Synchronization Interval

C,W

0

Specifies the periodic interval, in minutes, at which TimeSynchronization and UTCTimeSynchronization requests are sent. When set to zero, then periodic time synchronization is disabled.

Time Sync Recipients

W

 

Controls the restrictions placed on a device’s use of the Time Synchronization service. If the list is of length zero, a device is prohibited from automatically sending a Time Synchronization request. If the list is of length one or more, a device automatically sends a Time Synchronization request but only to the devices or addresses listed. If it is present, this attribute is writable. If the PICS indicates that this device is a Time Manager, then Time Synchronization Recipients is present.

Note: If PICS indicates the device is a Time Manager, this is required. If present, this attribute is writable.

UTC Offset

W

 

Indicates the number of minutes offset between local standard time and UTC. The time zones to the west of the zero degree meridian are positive and those to the east are negative. Subtract the value of the UTC Offset from the UTC received in the UTC Time Synchronization service requests to calculate the correct local standard time.

Range: -1440 though +1440

UTC Time Synchronization Recipients

C,W

 

Lists one or more BACnet recipients to which the device can issue a UTC Time Synchronization request. If the list is empty, the device cannot send a UTC Time Synchronization request to a BACnet recipient. The attribute requires several other parameters that define each recipient, such as its device ID, IP address information, or broadcast type and information.

VT Classes Supported

   

Contains a list of BACnet Video Terminal (VT) Classes that indicate a particular set of terminal characteristics. A device often supports multiple types of behaviors for differing types of terminals or differing types of operator interface programs. If either VT Classes Supported or Active VT Sessions is present, then both are present. Both are required if support of VT Services is indicated in the PICS.

Note: If either Video Terminal (VT) Classes Supported or Active VT Sessions is present, both are present. If the Protocol Implementation Conformance Statement (PICS) indicates support for VT Services, both of these attributes are present.

Vendor ID

    Distinguishes proprietary extensions to the protocol with a unique ASHRAE vendor ID code.

Vendor Name

    Identifies the manufacturer of the device.
1 If the device supports the backup and restore procedures, this attribute must be present and writable.