Trend Extensions - Metasys - LIT-1201793 - Software Application - Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Brand
Metasys
Product name
Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02
Language
English

The Trend Extension monitors and records the changes in the behavior of an individual attribute over time, thereby assisting you with diagnosing various system-wide behavioral characteristics. The Trend extension collects sample values at timed intervals or only upon changes in the given value. Trend data is still collected if the object is unreliable. The Trend extension continues to log data using the previous value preceded by ???, which indicates an unreliable status.

For example, use a Trend extension to collect data from the Analog Input object of a controller on the N2 Bus, which reports information such as outdoor air temperature or room air temperature.

Trend extensions are different from Trend Studies because Trend Studies query both the ADS and Engine for historical data. Trend Extensions query only the Engine.

Note: Although multiple trend extensions can be added to an object on an NxE, these extensions are combined as a single trend if sent to a Historical Data Repository. This may not yield the expected result. To use multiple trends on a single object in a Historical Data Repository, create duplicate AV or BV objects that map to the point in question, then create a new trend on the parallel AV or BV.

For trend performance information, refer to the Metasys System Configuration Guide (LIT-12011832).