Import Definition - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document type
User Guide
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

Menu Selection: Action > Import Definition

Imports the pre-built summary definition that is stored on the computer and is only available when the Summary Definitions folder is selected in the All Items tree. After importing a definition, the imported Summary Definitions appear in the Summary Definitions folder in the All Items tree.

Note: You also can import Summary Definitions that were previously exported. Refer to the Exporting a Summary Definition section in the SCT: System Configuration Tool Help (LIT-12011964) for more information.