Commanding an Item - Metasys - LIT-1201793 - Software Application - Metasys Site Management Portal - 12.0.50

Metasys Site Management Portal Help

Product
Building Automation Systems > Building Automation Systems > Metasys Site Management Portal
Document number
LIT-1201793
Version
12.0.50
Revision date
2023-06-02

About this task

To send a command to an item in a graphic, see the User Graphics Tool (UGT) section. To send a command to an item in a Graphics+ graphic, see the Graphics+ section. To send a command to multiple items, see the Commanding Multiple Items (Global Command) section.

To command an item:

Procedure

  1. Select the item to command in the navigation tree or in the display panel.
  2. From the Action Menu, select Command, or right-click and select Command.
  3. Filter the list of commands using the Show Command Set drop-down menu, if desired.
  4. Select the command to issue.
    Note: After selecting one of the available commands, you may be prompted to specify additional parameters for the command.
  5. Click Send.
    Note: If an error occurs while sending the command, the dialog box remains open.