In addition to the four modes of operation that determine the items appearing in menus, the Action menu is context-specific. Different item-specific options appear in the Action menu based on what is currently selected in the navigation tree. Also, different feature-specific options appear in the Action menu based on the active panel or feature displayed in the selected display panel.
Note: The options available in the Action Menu are also available from the Right-click
functionality.
The following table lists the menu items for the Action menu. For details on which options appear with certain items or features selected, see:
Click one of the following menu items for a description of the menu item.
|
Menu Item |
||
|---|---|---|
1 The commands in the Command dialog
require authorization.
3 Available on the Metasys Server
only.
4 Available for the Summary Definitions
folder in the All Items tree.