Summary of Changes - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 13.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
13.0
Revision date
2024-03-26
Product status
Active

The following information is new or revised:

  • Added support for Windows® 11 Pro and Enterprise (21H2, 22H2)
  • Added support for Windows® Server 2022
  • Added support for SQL® Server 2022
  • Removed support for Windows® Server 2016
  • Removed support for SQL Server 2016 and SQL Server 2016 Express
  • Added information that all uninstallers incorporate a list and descriptions for which databases are removed when you uninstall SCT or SMP.