Uninstalling Metasys Server Software - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 13.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
13.0
Revision date
2024-03-26
Product status
Active

Follow the steps in this section for uninstalling the current version of Metasys Server software from a computer. However, if you have Metasys Server software at Release 8.x or later, and you intend to install Release 13.0, you can skip this section and go directly to Upgrading Metasys Server. The only exception is if you are upgrading to a different software build of the Metasys Server at the same release level (for example, 11.0.0.4570 to 11.0.0.5847). In this case, you must first uninstall the ADS/ADX software, then install the newer build.

Note: The Remove databases option on the uninstall screen is selected by default. If you check this box, the XMS database, which stores site configuration data is removed during uninstall process. No other databases except the XMS database are removed. To retain this database, uncheck that selection before starting the uninstallation.
  1. In Control Panel, click Programs > Programs and Features. A list of all installed programs appears.
  2. Locate and select the installed release of the Metasys Server program item.
  3. Click Uninstall. The removal process begins. It may take a few moments before the first uninstall window appears.
    Figure 1. Uninstall Window

    1. Remove databases: check if you want to remove the XMS database during the uninstallation. No other databases except the XMS database are removed. For more information about the databases, hover over the info icon next to the database name.
    2. Windows authentication: check if you want to use Windows authentication for uninstalling the software; uncheck if you want to use a SQL Server administrator account. Enter a SQL Server username and password.
    3. Username: specify the user name of the SQL Server administrator. This field is enabled only if Windows authentication is not checked.
    4. Password: specify the password of the SQL Server administrator. This field is enabled only if Windows authentication is not checked.
  4. Click Uninstall. The progress screen appears. Wait until all steps have finished.
  5. After all steps have completed, the complete box appears.
    1. Click Restart Now: a restart is needed to make the changes on your computer.
    2. Click Finish: a restart is not needed.