|
Supported Operating System |
Supported Database Options |
|---|---|
|
Windows® Server® 2022 (64-bit) Windows® Server® 2019 (version 1809 or later) (64-bit) |
SQL Server® 2022 (64-bit) SQL Server® 2019 with CU18 (64-bit) SQL Server® 2017 with CU31 (64-bit) |
Use the steps in the following table for upgrading the database component of the ADX on a split Metasys system.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify that the
computer intended for Metasys Server software is running one of the following supported
Windows Server operating systems:
|
Open a command prompt window and run the command Winver as Administrator. The Windows version is listed in the dialog box that appears. Start Windows Update from the Search box and apply all required and recommended updates before installing any Metasys software. |
|
2. |
Configure the Windows Firewall to ensure the ports that Metasys software requires are open. |
|
|
3. |
Install Microsoft .NET Framework 3.5 if the computer does not have this software installed. |
In Control Panel, click Programs > Programs and Features > Turn Windows features on and off. The Server Manager window appears. Use the Add Roles and Features Wizard in Server Manager to add the .NET Framework 3.5 Features and HTTP Activation components. On some server-class OSs, HTTP Activation may be listed under WCF Services. |
| 4. |
Make sure all required software components are enabled. |
See Required Windows operating system roles and features for more information. |
|
5. |
If you are installing the Metasys Server software on an English language computer, skip to the next step. If you are installing the Metasys Server software on a non-English language computer, you need to set the computer's regional settings and the default language used by the SQL Server database to the same locale as the site default language. |
Consult the Microsoft documentation and see Installing Metasys server for a non-English locale. |
|
6. |
Install a version of SQL Server Standard or Enterprise software on the computer that the Metasys system supports. Make sure you include the Database component, but you do not need to install the Reporting Services component. |
Refer to SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
7. |
As part of performing an out-of-place upgrade, disconnect the old database computer and web/application computer from the building network, then connect the new database computer and web/application computer to the building network. Then, follow the steps to the right. |
|
|
8. |
(OPTIONAL) If you need the server to be FIPS compliant, enable FIPS mode and install the Metasys FIPS component. |
|
|
9. |
Create a full disk image backup of the computer's hard drive to external media (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |
|
10. |
Go to the next section to upgrade the web/application server of the split ADX. |
Go to Web/Application Server. |