Metasys Server Out-of-Place Upgrade - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 13.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
13.0
Revision date
2024-03-26
Product status
Active

This section includes the steps for performing an out-of-place upgrade of the ADS or ADX software to Metasys Server 13.0. An out-of-place upgrade applies in either of these two scenarios: (1) you need to reformat the computer that is currently running the Metasys system to a new, supported Windows operating system before performing the upgrade or (2) you need to move the current Metasys system to a different computer or virtual machine during the upgrade. Before upgrading to Metasys Server 13.0 software, make sure you review Pre-Work checklist for new installations and upgrades and Out-of-Place Upgrade Considerations.

Which type of Metasys Server are you upgrading?
Unified ADS Select to upgrade a Metasys Server on a desktop operating system.
Unified ADS with SCT Select to upgrade a Metasys Server and SCT on a desktop operating system.
Unified ADX Select to upgrade a Metasys Server on a server-class operating system.
Unified ADX with SCT Select to upgrade a Metasys Server and SCT on a server-class operating system.
Split ADX with SCT Select to upgrade a Metasys Server and SCT on a split configuration. With a split ADX, the database component is installed on one server-class system, the web/application component is installed on another server-class operating system, and SCT is installed on either a server-class or desktop operating system.