|
Supported Operating System |
Supported Database Options |
|---|---|
|
Windows® Server® 2022 (64-bit) Windows® Server® 2019 (version 1809 or later) (64-bit) |
SQL Server® 2022 (64-bit) SQL Server® 2019 with CU18 (64-bit) SQL Server® 2017 with CU31 (64-bit) Note: If you are not installing Reporting Services, you do not require SQL
Server on the Web/Application computer.
|
Use the steps in the following table for installing the web/application component of the ADX on a split Metasys system.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify that the
computer intended for Metasys Server software is running one of the following supported
Windows Server operating systems:
|
Open a command prompt window and run the command Winver as Administrator. The Windows version is listed in the dialog box that appears. Start Windows Update from the Search box and apply all required and recommended updates before installing any Metasys software. |
|
2. |
Verify that the computer name is valid for Metasys Server software. |
In Control Panel, click System and Security > System and verify the computer name that
appears in the window meets the following criteria:
|
|
3. |
Configure the Windows Firewall to ensure the ports that Metasys software requires are open. |
|
|
4. |
Follow the appropriate
step:
|
Consult the Microsoft documentation and see Installing Metasys server for a non-English locale. |
|
5. |
Install Microsoft .NET Framework 3.5 if the computer does not have this software feature installed. |
On
the start screen, click Server Manager. Select Add roles and features. The
Add Roles and Features Wizard opens. Follow the wizard until you reach the
Features section. Click the Microsoft .NET Framework
3.5 or .NET Framework 3.5 feature. Check the HTTP Activation component. If you do not have Internet access, insert
the operating system media, open a Command prompt with Run as Administrator, and execute
this command (where <drive> is the disk drive with the media): |
| 6. |
If you intend to use the Metasys Advanced Reporting System, install SQL Server 2017 and then install and configure SQL Server Reporting Services. Use the standalone Reporting Services installer. |
For the Reporting Services installer, download SQL Server 2017 Reporting Services. |
|
7. |
If you plan to use the Metasys Advanced Reporting system on an ADX that will include any non-English languages, install the corresponding language support files for SQL Server's reporting services. |
Refer to the Appendix: Reporting Services Language Support for Metasys Advanced Reporting System of SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
8. |
If you want the Metasys Server to use trusted certificates instead of self-signed certificates (the default), configure the certificates on the Metasys Server before installing the software. Otherwise, go to the next step. |
|
|
9. |
Install the Metasys Server software, selecting the database server for the database component of the split ADX, the web/application server for the Metasys Reporting component of the split ADX, and the remote SCT and Data server systems for the Metasys Advanced Reporting feature. |
See Installing Metasys Server: Custom Method. |
|
10. |
License the Metasys ADX software with the Software Manager |
Refer to the Software Manager Help (LIT-12012389). |
| 11. |
Start Metasys UI to verify proper operation. |
Metasys UI Help (LIT-12011953) |
| 12. |
(Optional) License SMP software. |
Refer to Metasys Software Purchase Options Product Bulletin (LIT-12011703) |
|
13. |
Install and license any other Metasys software (for example, Metasys Export Utility). |
Refer to their respective installation documents. |
|
14. |
(Optional) Start Launcher and add a profile for the Site Management Portal (SMP). |
Refer to Launcher Help (LIT-12011742) . |
|
15. |
(Optional) Start Metasys SMP from the Launcher and verify proper operation. |
|
|
16. |
(Optional) If you want to move the Metasys historical databases now, use SQL Management Studio to move the databases to your chosen location. |
See Moving Metasys Historical Databases to a Custom Location. |
|
17. |
If prompted, restart the computer. |
Use the standard procedure to restart the operating system. |
| 18. |
(Optional) If you need the server to be FIPS compliant, enable FIPS mode and install the Metasys FIPS component. |