|
Supported Operating System |
Supported Database Options |
|---|---|
|
Windows® Server® 2022 (64-bit) Windows® Server® 2019 (version 1809 or later) (64-bit) |
SQL Server® 2022 (64-bit) SQL Server® 2019 with CU18 (64-bit) SQL Server® 2017 with CU31 (64-bit) |
Use the steps in the following table for installing the database component of the ADX on a split Metasys system.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify that the
computer intended for Metasys Server software is running one of the following supported
Windows Server operating systems:
|
Open a command prompt window and run the command Winver as Administrator. The Windows version is listed in the dialog box that appears. Start Windows Update from the Search box and apply all required and recommended updates before installing any Metasys software. |
|
2. |
Configure the Windows Firewall to ensure the ports that Metasys software requires are open. |
|
|
3. |
Follow the appropriate
step:
|
Consult the Microsoft documentation and see Installing Metasys server for a non-English locale. |
|
4. |
Install Microsoft .NET Framework 3.5 if the computer does not have this software feature installed. |
On
the start screen, click Server Manager. Select Add roles and features. The
Add Roles and Features Wizard opens. Follow the wizard until you reach the
Features section. Click the Microsoft .NET Framework
3.5 or .NET Framework 3.5 feature. Check the HTTP Activation component. If you do not have Internet access, insert
the operating system media, open a Command prompt with Run as Administrator, and execute
this command (where <drive> is the disk drive with the media): |
| 5. |
Install a supported version of SQL Server Standard or Enterprise software, including the recommended cumulative update, if any. Select the Database Engine Services and Management Tools components. |
Refer to SQL Server Installation and Upgrade Instructions (LIT-12012240). |
| 6. |
(Optional) Install the Metasys Database Manager. |
Refer to the Metasys Database Manager Installation Guide (LIT-12011553) . |
|
7. |
If prompted, restart the computer. |
Use the standard procedure to restart the operating system. |
|
8. |
Go to the next section to install the web/application server of the split ADX. |
Go to Web/Application Server. |