This section includes the steps for installing Metasys Server software. Before you begin the installation process, make sure you review Pre-Work checklist for new installations and upgrades.
If you instead need to upgrade existing Metasys Server software, see Metasys Server In-Place Upgrade or Metasys Server Out-of-Place Upgrade.
Which type of Metasys Server are you installing? | |
---|---|
Unified ADS | Select to install the Metasys Server on a desktop operating system. |
Unified ADS with SCT | Select to install the Metasys Server and SCT on a desktop operating system. |
Unified ADX | Select to install the Metasys Server on a server-class operating system. |
Unified ADX with SCT | Select to install the Metasys Server and SCT on a server-class operating system. |
Split ADX with SCT | Select to install a split Metasys Server where database component is installed on one server-class system, the web/application component is installed on another server-class operating system, and SCT is installed on a desktop or server-class operating system. |