Software Component |
Product |
Where to Obtain |
|
---|---|---|---|
Operating System (select one) 1 |
|||
Windows® 11 Pro and Windows® 11 Enterprise versions 22H2, 21H2 (64-bit) General Availability Channel (GAC) |
ADS /SCT |
Microsoft Corporation |
|
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). 2 |
|||
Windows® Server® 2022 (64-bit) |
ADX /SCT |
||
Windows® Server® 2019 (version 1809 or later) (64-bit) |
|||
Operating System (OS) Components (installed by Metasys Server) |
|||
Internet Information Services (IIS) (included with OS) |
ADS/ADX /SCT |
OS media |
|
Microsoft Message Queuing (MSMQ) |
|||
Miscellaneous (select all) |
|||
Microsoft .NET Framework 3.5 SP1 or 3.5.1 |
ADS/ADX /SCT |
OS Media |
|
Microsoft .NET Framework 4.7.2 or Microsoft .NET Framework 4.8 (installed by Metasys Server) |
Microsoft Corporation |
||
Microsoft .NET 6.0.16 (installed by Metasys Server) |
Microsoft Corporation |
||
Database (select one) |
|||
SQL Server® 2022 Express (64-bit) |
ADS /SCT |
||
SQL Server® 2019 Express with CU18 (64-bit) |
|||
SQL Server® 2017 Express with CU31 (64-bit) |
|||
SQL Server® 2022 (64-bit) |
ADX /SCT |
Microsoft Corporation |
|
SQL Server® 2019 with CU18 (64-bit) 3 (Standard or Enterprise Edition) |
|||
SQL Server® 2017 with CU31 (64-bit) 3 (Standard or Enterprise Edition) |
|||
Database Tools |
|||
SQL Installer Tool |
ADS /SCT |
||
Microsoft SQL Server Management Studio |
|||
Reporting Services (optional) |
|||
Microsoft Report Viewer 2012 Redistributable Package |
ADX | ||
SQL Server Reporting Services (SSRS) for SQL Server 2017 |
Microsoft Corporation |
Before you begin with the Metasys Server installation or upgrade, review Table 1 to verify
that you have the required software. The table also indicates where you can obtain each software
component.
Note: If you purchased Metasys
Server software that includes SQL Server software (for example, MS-ADX25SQL-0), the SQL Server
package is provided in a .zip file. Simply use a file extraction tool such as WinZip™ or 7-Zip
File Manager to extract the .zip file to the server's hard drive.
Note: Do not install Metasys on a
Domain Controller. A Domain Controller provides the Active Directory service to network users
and computers; stores directory data; and manages user and domain interactions including the
login process, authentication, and directory searches.
1 We advise that the computer you
want to use for Metasys software had its operating system installed on a cleanly formatted
hard disk. If you use a computer that was upgraded from a previous version of Windows,
files and registry settings left behind after the upgrade may adversely affect the
installation of Metasys system software.
2 Metasys system
software does not support the touchscreen interface that is featured in the Windows 10 and
Windows 11 operating systems.
3 At Release 13.0, Metasys Advanced Reporting System is compatible with SQL Server 2017
software, but is not compatible with SQL Server 2019 or SQL Server 2022.
4 Required for reports generated by the
Metasys Advanced Reporting System. Use Report Viewer 2012 Redistribution Package for SQL
Server 2017.