The following table lists by operating system the SQL Server software editions that have been fully qualified by Johnson Controls for the current release of Metasys Server. You can select other combinations, but for best performance, select from the following pairings.
Operating System |
Database Software |
||||||
---|---|---|---|---|---|---|---|
Desktop Computer Platform |
Server Computer Platform |
||||||
SQL Server® 2022 Express (64-bit) |
SQL Server® 2019 Express with CU18 (64-bit) |
SQL Server® 2017 Express with CU31 (64-bit) |
SQL Server® 2022 (64-bit) | SQL Server® 2019 with CU18 (64-bit) | SQL Server® 2017 with CU31 (64-bit) | ||
Desktop |
Windows® 11 Pro and Windows® 11 Enterprise versions 22H2, 21H2 (64-bit) General Availability Channel (GAC) |
x |
x |
x |
|||
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). |
x |
x |
x |
||||
Server |
Windows® Server® 2022 (64-bit) |
x |
x |
x |
|||
Windows® Server® 2019 (version 1809 or later) (64-bit) |
x |
x |
x |