The Metasys Server requires a software license for its base product. An application called Software Manager, installed with Metasys Server software, manages Metasys software licenses on a machine. License the Metasys Server software immediately after installation. Also installed with the Metasys Server are Fault Detection, Fault Triage, and the Monitoring and Commanding API, which are optional features that you need to purchase and license separately. Metasys UI, however, does not require a separate license. For information about activating licenses, refer to the Starting a license activation section in the Software Manager Help (LIT-12012389).
Note:
SMP UI access to
Release 12.0 and later Metasys Servers requires an SMP license except for an ADX
with MVE installed and licensed.