Removing or rebinding the secure certificate - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 13.0

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document number
LIT-12012162
Version
13.0
Revision date
2024-03-26
Product status
Active

About this task

Follow these steps to remove a certificate binding from a Metasys server or SCT computer or to change a certificate binding. If you are changing a binding, the binding must already exist on the server from which to select.

Procedure

  1. In Control Panel, select System and Security > Administrative Tools and double-click Internet Information Services (IIS) Manager. The IIS main screen appears.
  2. Expand the Connections in the left pane so that Default Web Site appears. Click Default Web Site.
  3. On the Actions pane, click Bindings under Edit Site. The Site Bindings screen appears.
  4. To remove the site binding, select it from the list and click Remove. A user prompt appears to verify that you want to remove the selected binding. Click Yes to remove or No to cancel.

    To rebind the certificate, select it from the list and click Edit. The Edit Site Binding screen appears.

  5. Click Select to open a table that lists all certificates available for binding.
  6. Select the binding from the table and click OK. The Edit Site Binding screen appears with the newly selected binding.
  7. Click OK to save the binding change.