Uninstalling the Metasys Server Software Introduction - Metasys - LIT-12012162 - MS-ADS05U-0 MS-ADX10U-0 MS-ADX10SQL-0 MS-ADX25U-0 MS-ADX25SQL-0 MS-ADX50U-0 MS-ADX50SQL-0 MS-ADX50SQL2-0 MS-ADX100U-0 MS-ADX100SQL2-0 - Server - Metasys Server - 12.0.50

Metasys Server Installation and Upgrade Instructions

Product
Building Automation Systems > Application Servers > Metasys Server
Document type
Installation Guide
Document number
LIT-12012162
Version
12.0.50
Revision date
2023-10-12
Product status
Active
Important: If you receive error messages when you uninstall Metasys Server (ADS/ADX) software, you may have problems reinstalling it. Diagnose these problems before you attempt to reinstall the software.
Important: The Metasys Server is offline from when you uninstall the software to when you finish the upgrade or reinstallation. Be aware that if your historical databases are over 500 MB, the upgrade may take several hours to complete. Consider using the Metasys Database Manager or SQL Server software tools to purge your historical database prior to an upgrade. Refer to the Metasys Database Manager Help (LIT-12011202) for details.
Note: The Metasys Server software must be able to communicate with the SQL Server databases during the uninstallation process.