|
Supported Operating System |
Supported Database Options |
|---|---|
|
Windows® Server® 2019 (version 1809 or later) (64-bit) Windows® Server® 2016 (version 1607 or later) (64-bit) |
SQL Server® 2019 with CU19 (64-bit) SQL Server® 2017 with CU31 (64-bit) SQL Server® 2016 with SP3 GDR (64-bit) |
Use the steps in the following table to perform an out-of-place upgrade of Metasys Server and SCT software on a computer with a server operating system. These steps presume that the computer currently has no Metasys software installed.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify that the computer
intended for Metasys Server software is running one of the following supported Windows
Server operating systems:
|
Open a command prompt window and run the command Winver as Administrator. The Windows version is listed in the dialog box that appears. Start Windows Update from the Search box and apply all required and recommended updates before installing any Metasys software. |
|
2. |
Verify that the computer name is valid for Metasys Server software. |
In Control Panel, click System and Security > System and verify the computer name that
appears in the window meets the following criteria:
|
|
3. |
Configure the Windows Firewall to ensure the ports that Metasys software requires are open. |
|
|
4. |
If you are installing the Metasys Server software on an English language computer, skip to the next step. If you are installing the Metasys Server software on a non-English language computer, you need to set the computer's regional settings and the default language used by the SQL Server database to the same locale as the site default language. |
Consult the Microsoft documentation and see Installing Metasys server for a non-English locale. |
|
5. |
If the computer has multiple network cards, configure the network card that the Metasys Server software is to use. |
|
|
6. |
Install Microsoft .NET Framework 3.5 if the computer does not have this software installed. |
In Control Panel, click Programs > Programs and Features > Turn Windows features on and off. The Server Manager window appears. Use the Add Roles and Features Wizard in Server Manager to add the .NET Framework 3.5 Features and HTTP Activation components. On some server-class OSs, HTTP Activation may be listed under WCF Services. |
| 7. |
Make sure all required software components are enabled. |
See Required Windows operating system roles and features for more information. |
|
8. |
Install a version of SQL Server Standard or Enterprise software on the computer that the Metasys system supports. Install these components: Database Engine Services, Management Tools, and if you plan to install Metasys Advanced Reporting Services, install Reporting Services. |
Refer to SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
9. |
If you plan to install Metasys Advanced Reporting System, verify that Reporting Services on the computer is configured properly. |
Refer to the Verifying SQL Server Reporting Services Configuration section of SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
10. |
Install support files on the computer if you plan to offer the Site Management Portal in languages other than English. |
Refer to the Appendix: Reporting Services Language Support for Metasys Advanced Reporting System of SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
11. |
Upload and back up all Metasys Server and network engine archive databases to the existing SCT. Make sure you select the Include Security option for the upload. |
Refer to Database Uploading, Downloading, and Synchronization of SCT: System Configuration Tool Help (LIT-12011964) or the SCT Technical Bulletin (LIT-1201534) for the release you have currently installed (not the new release). |
|
12. |
Forward all trend samples from each network engine to the Metasys Server Site Director by using the Route Samples command at each engine. This step ensures that the Site Director has all possible samples before you begin the upgrade. Wait a few minutes to ensure that all samples have been forwarded. |
Refer to Metasys Site Management Portal Help (LIT-1201793) for information about the Route Samples command. |
|
13. |
Stop the Metasys III Device Manager service on the Metasys Server computer. This action prevents the collection of any new audits, alarms, trends, and annotations while you perform the upgrade. If the customer can accept the loss of data samples during an upgrade, you can skip to the next step. |
Right-click the Windows taskbar and start Task Manager. Click the Services tab. Locate a service called Metasys III Device Manager. Select this service and right-click and select Stop Service. The Metasys III Device Manager service stops. |
|
14. |
Perform a complete backup of all historical data in the Metasys Server computer with the Metasys Database Manager. If the system to be upgraded is at Release 8.0 or 8.1, after the historical databases are backed up, use the SQL Server Management Studio to backup the SpacesAuthorization database. After the installation is complete, restore the SpacesAuthorization database. |
Refer to Backing Up a Database in Metasys Database Manager Help (LIT-12011202) . |
|
15. |
Make a copy of each historical database backup file and archive backup file and store them on removable media for example, a flash drive or DVD. |
Use Windows Explorer to prepare and archive the file copies. |
|
16. |
Select the appropriate action:
|
|
|
17. |
As part of performing an out-of-place upgrade, follow the steps to the right. |
|
|
18. |
Install the Metasys Server 12.0.50 software. |
|
|
19. |
License the Metasys Server software and SMP software with the Software Manager. |
Refer to the Software Manager Help (LIT-12012389). |
|
20. |
Install and license any other Metasys Release 12.0.50 software at this time, including the Metasys Export Utility. |
Refer to their respective installation documents. For licensing, refer to the Software Manager Help (LIT-12012389). |
| 21. |
Install any other Metasys software at this time, including the Metasys Export Utility and MVE. |
Refer to their respective installation documents. For MVE, see Installing MVE Software. |
|
22. |
Start Launcher on the computer and launch the Site Management Portal (SMP) for the upgraded Metasys Server. |
Refer to Launcher Tool Help (LIT-12011742) . |
|
23. |
To verify Metasys Server operation, log in to the Metasys Server using the MetasysSysAgent user and password. |
|
|
24. |
Start Launcher on the computer, and add a profile for Metasys SCT. |
Refer to Launcher Tool Help (LIT-12011742) . |
|
25. |
Log in to SCT 15.0 and open the archive database. Allow SCT to upgrade the database to Release 15.0. |
Refer to SCT: System Configuration Tool Help (LIT-12011964) . |
| 26. |
Log on to SCT 15.0, then use the Manage Archive wizard to upgrade the ADS/ADX device to Release 12.0. When asked to enter the Metasys Server user credentials, specify the MetasysSysAgent user and password. If during the upgrade process an Upgrade Warning dialog box appears regarding password resets, set a default password for the affected users, then contact the users of their new default password. Each affected user is prompted to change this default password when logging on to the Metasys Server 12.0.50 for the first time. |
Refer to SCT: System Configuration Tool Help (LIT-12011964) . |
|
27. |
Select the appropriate action:
|
Refer to the Security Administrator System Technical Bulletin (LIT-1201528) . |
| 28. |
If you upgraded the ADS/ADX device in your SCT archive from a Metasys
version prior to Release 12.0, to Release 12.0, confirm the following:
|
To check the configuration of the Third party BBMDs, see Checking third party BBMDs compatibility for ADS/ADX upgrades. To check the configuration of the Email DDA destinations, see Checking email DDA compatibility for ADS/ADX upgrades.
Note: The archive download to a Release 12.0 ADS/ADX fails if these
attributes have an incompatible configuration. For more information, see General Troubleshooting.
|
|
29. |
Download the Site Director
archive database from SCT 15.0 to the Metasys Server Site Director, making sure that you
click Include Security. When asked to enter the Metasys Server user
credentials, specify the MetasysSysAgent user and password. If the login for the Metasys
Server fails, click the Clear Security Database tab and click Set to be cleared. The device is upgraded, but the security database
is removed from the archive.
Note: A Server download logs off Metasys
UI and SMP users.
Note: Before you attempt a
download/upload to the server from SCT, wait for it to become operational. If you perform
a download/upload before then, the server does not operate correctly. To fix this, restart
the Metasys server host, wait for it to become operational, and try the process
again.
|
Refer to Database Uploading, Downloading, and Synchronization in SCT: System Configuration Tool Help (LIT-12011964) for information on downloading. |
|
30. |
(Optional) If you want to move the Metasys historical databases now, use SQL Management Studio to move the databases to the desired location. |
See Moving Metasys Historical Databases to a Custom Location. |
|
31. |
Update the network engines that
you want to upgrade to Release 12.0.
Note: If you are upgrading from
Release 5.2 or later, you do not need to update all devices to the newer release (except
the Site Director). SCT 15.0 supports devices at multiple Metasys software releases,
beginning with Release 5.2.
|
Refer to NAE Update Tool Help (LIT-12011524) and SCT: System Configuration Tool Help (LIT-12011964) . |
|
32. |
If you updated network engines to Release 12.0, use SCT 15.0 to download the archive database of each network engine. The download also restores the Security database. After the download completes, issue the Reset Device command to each downloaded N40-class device (NxE35, NIE39, NxE45, NIE49, NxE25, or NIE29s) to ensure that the security database is archived to non-volatile memory. This step is new beginning at Release 8.0, but is not required for any other network engine (for example, NxE55s, NxE59s, SNEs, and SNCs). |
Refer to Database Uploading, Downloading, and Synchronization in SCT: System Configuration Tool Help (LIT-12011964) for information on downloading. |
|
33. |
Create a full disk image backup of the computer's hard drive to external media (optional but recommended). |
Refer to the documentation that came with your operating system backup software. |