|
Supported Operating System |
Supported Database Options |
|---|---|
|
Windows® Server® 2019 (version 1809 or later) (64-bit) Windows® Server® 2016 (version 1607 or later) (64-bit) |
SQL Server® 2019 with CU19 (64-bit) SQL Server® 2017 with CU31 (64-bit) SQL Server® 2016 with SP3 GDR (64-bit) |
Use the steps in the following table for installing the web/application component of the ADX on a split Metasys system.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify that the
computer intended for Metasys Server software is running one of the following supported
Windows Server operating systems:
|
Open a command prompt window and run the command Winver as Administrator. The Windows version is listed in the dialog box that appears. Start Windows Update from the Search box and apply all required and recommended updates before installing any Metasys software. |
|
2. |
Verify that the computer name is valid for Metasys Server software. |
In Control Panel, click System and Security > System and verify the computer name that
appears in the window meets the following criteria:
|
|
3. |
Configure the Windows Firewall to ensure the ports that Metasys software requires are open. |
|
|
4. |
Follow the appropriate
step:
|
Consult the Microsoft documentation and see Installing Metasys server for a non-English locale. |
|
5. |
If the computer has multiple network cards, configure the network card that the Metasys Server software is to use. |
|
|
6. |
Install Microsoft .NET Framework 3.5 if the computer does not have this software feature installed. |
In Control Panel, click Programs > Programs and Features > Turn Windows features on and off. Click the
Microsoft .NET Framework 3.5 or .NET Framework 3.5 feature.
Check the HTTP Activation component. If you do not have Internet
access, insert the operating system media, open a Command prompt with Run as Administrator,
and execute this command (where <drive> is the disk drive with the media): On server-class OSs, use the Add Roles and Features Wizard in Server Manager to add the .NET Framework 3.5 Features and HTTP Activation components. On some server-class OSs, HTTP Activation may be listed under WCF Services. |
|
7. |
Make sure all required software components are enabled. |
See Required Windows operating system roles and features for more information. |
|
8. |
Install
a version of SQL Server Reporting Services that matches the version of SQL installed on
the database server. If you are using SQL Server 2016, select the Reporting Services and Management Tools components, but not
the Database Engine Services component. If you are using SQL Server 2017, use the standalone
Reporting Services installer.
Note:
Metasys Advanced Reporting System does not support SQL Server
2019.
|
Refer to SQL Server Installation and Upgrade Instructions (LIT-12012240). For the Reporting Services installer, download SQL Server 2017 Reporting Services. |
|
9. |
If you intend to use the Metasys Advanced Reporting System, configure Reporting Services. |
Refer to the Configuring SQL Server Reporting Services for the Metasys Advanced Reporting System section of SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
10. |
Install support files if you plan to offer the Site Management Portal in languages other than English. |
Refer to the Appendix: Reporting Services Language Support for Metasys Advanced Reporting System of SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
11. |
If you want the Metasys Server to use trusted certificates instead of self-signed certificates (the default), configure the certificates on the Metasys Server before installing the software. Otherwise, go to the next step. |
|
|
12. |
Install the Metasys Server software, selecting the database server for the database component of the split ADX, the web/application server for the Metasys Reporting component of the split ADX, and the remote SCT and Data server systems for the Metasys Advanced Reporting feature. |
See Installing Metasys Server: Custom Method. |
|
13. |
License the Metasys ADX software with the Software Manager |
See Licensing the Metasys Server Software, including steps for enabling and installing FIPS and for installing the MVE software |
| 14. | Install and license any other Metasys software at this time, including the Metasys Export Utility and MVE. |
Refer to their respective installation documents. For MVE, see Installing MVE Software. |
| 15. |
Start Metasys UI to verify proper operation. |
Metasys UI Help (LIT-12011953) |
| 16. |
(Optional) License SMP software. Note: An SMP license is not required if MVE is
installed and licensed.
|
Refer to Metasys Software Purchase Options Product Bulletin (LIT-12011703) |
|
17. |
(Optional) Start Launcher and add a profile for the Site Management Portal (SMP). |
Refer to Launcher Tool Help (LIT-12011742) . |
|
18. |
(Optional) Start Metasys SMP from the Launcher and verify proper operation. |
|
|
19. |
(Optional) If you want to move the Metasys historical databases now, use SQL Management Studio to move the databases to the desired location. |
See Moving Metasys Historical Databases to a Custom Location. |
|
20. |
If prompted, restart the computer. |
Use the standard procedure to restart the operating system. |
|
21. |
(Optional) If you need the server to be FIPS compliant, enable FIPS mode and install the Metasys FIPS component. |