Refer to the SCT Installation and Upgrade Instructions (LIT-12012067) for more information on supported platforms and for installing SCT.
Use the steps in the following table for installing SCT on a split Metasys system.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify
that the computer intended for SCT software is running one of the following supported
operating systems:
|
Open a command prompt window and run the command Winver as Administrator. The Windows version is listed in the dialog box that appears. Start Windows Update from the Search box and apply all required and recommended updates before installing any Metasys software. |
|
2. |
Configure the Windows Firewall to ensure the ports that Metasys software requires are open. |
|
|
3. |
Follow the appropriate
step:
|
Consult the Microsoft documentation and see Installing Metasys server for a non-English locale. |
|
4. |
If the computer has multiple network cards, configure the network card that the Metasys Server software is to use. |
|
|
5. |
Install Microsoft .NET Framework 3.5 if the computer does not have this software feature installed. |
In Control Panel, click Programs > Programs and Features > Turn Windows features on and off. Click the
Microsoft .NET Framework 3.5 or .NET Framework 3.5 feature.
Check the HTTP Activation component. If you do not have Internet
access, insert the operating system media, open a Command prompt with Run as Administrator,
and execute this command (where <drive> is the disk drive with the media): On server-class OSs, use the Add Roles and Features Wizard in Server Manager to add the .NET Framework 3.5 Features and HTTP Activation components. On some server-class OSs, HTTP Activation may be listed under WCF Services. |
| 6. |
Make sure all required software components are enabled. |
See Required Windows operating system roles and features for more information. |
|
7. |
Install a supported version of SQL Server software on a server class machine, including the recommended cumulative update, if any. The SCT setup installs SQL Server 2019 Express with CU18 on a non-server box if no SQL is present. |
Refer to SQL Server Installation and Upgrade Instructions (LIT-12012240). |
|
8. |
If you want the Metasys SCT to use trusted certificates instead of self-signed certificates (the default), configure the certificates on the Metasys SCT before installing the software. Otherwise, go to the next step. |
|
|
9. |
Install and license SCT 15.0 software. |
Refer to the SCT Installation and Upgrade Instructions (LIT-12012067) . |
| 10. |
Install and license Metasys Device Packages, Metasys Field Controller Packages, and Johnson Controls SA Bus Device Packages |
Refer to the Software Manager Help (LIT-12012389) |
|
11. |
Start Launcher and add a profile for Metasys SCT. |
Refer to Launcher Tool Help (LIT-12011742) . |
|
12. |
Start Metasys SCT from Launcher. If you will be installing Metasys Advanced Reporting, create a new archive that you can later select in the Reporting tab of the Metasys Server setup window. |
Refer to the SCT Installation and Upgrade Instructions (LIT-12012067) . |
|
13. |
Go to the next section to install the database server of the split ADX. |
Go to Database Server. |