|
Supported Operating System |
Supported Database Options |
|---|---|
|
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). For all future Windows 10 updates after version 22H2, Johnson Controls will evaluate and certify that Metasys software can support the updates before we provide guidance on support. |
SQL Server® 2019 Express with CU19 (64-bit) SQL Server® 2017 Express with CU31 (64-bit) SQL Server® 2016 Express with SP3 GDR (64-bit) |
Use the steps in the following table for installing and configuring the Metasys Server software on a computer with a desktop operating system.
|
Step |
Action |
Reference or Additional Steps |
|---|---|---|
|
1. |
Verify that
the computer intended for Metasys Server software has one of the following supported Windows
desktop operating systems:
|
Open a command prompt window and run the command Winver as Administrator. The Windows version is listed in the dialog box that appears. Start Windows Update from the Search box and apply all required and recommended updates before installing any Metasys software. |
|
2. |
Verify that the computer name is valid for Metasys Server software. |
In Control Panel, click System and Security > System and verify the computer name that
appears in the window meets the following criteria:
|
|
3. |
Configure the Windows Firewall to ensure the ports that Metasys software requires are open. |
|
|
4. |
Follow the appropriate
step:
|
Consult the Microsoft documentation and see Installing Metasys server for a non-English locale. |
|
5. |
If the computer has multiple network cards, configure the network card that the Metasys Server software is to use. |
|
|
6. |
Install Microsoft .NET Framework 3.5 if the computer does not have this software feature installed. |
In Control Panel, click Programs > Programs and Features > Turn Windows features on and off. Click the
Microsoft .NET Framework 3.5 or .NET Framework 3.5 feature.
Check the HTTP Activation component. If you do not have Internet
access, insert the operating system media, open a Command prompt with Run as Administrator,
and execute this command (where <drive> is the disk drive with the media): |
| 7. |
Make sure all required software components are enabled. |
See Required Windows operating system roles and features for more information. |
| 8. |
Select the appropriate
action:
|
See Specifying Custom Locations for Metasys Server Application and Databases. This section explains how to install SQL Server software and SQL Server Management Studio to the alternate disk drive (for example, E: drive). After completing the SQL Server installation steps, follow the next step below. |
| 9. |
If you want the Metasys Server to use trusted certificates instead of self-signed certificates (the default), configure the certificates on the Metasys Server before installing the software. Otherwise, go to the next step. |
|
|
10. |
Install the Metasys Server software, which also installs a supported version of SQL Server software. |
See Installing Metasys Server: Default Method . However, if you want to install to an alternate disk drive, see Installing Metasys Server: Custom Method. |
|
11. |
License the Metasys ADS software with the Software Manager |
Refer to Metasys Software Purchase Options Product Bulletin (LIT-12011703) |
|
12. |
Start Metasys UI to verify proper operation. |
Metasys UI Help (LIT-12011953) |
|
13. |
(Optional) License SMP software. |
Refer to Metasys Software Purchase Options Product Bulletin (LIT-12011703) |
|
14. |
(Optional) Start Launcher and add a profile for the Site Management Portal (SMP). |
Refer to Launcher Tool Help (LIT-12011742) . |
|
15. |
(Optional) Start Metasys SMP from the Launcher and verify proper operation. |
|
|
16. |
(Optional) If you want to move the Metasys historical databases now, use SQL Management Studio to move the databases to the desired location. |
See Moving Metasys Historical Databases to a Custom Location. |
|
17. |
(Optional) Install the Metasys Database Manager.
Note: Metasys Database Manager is not FIPS
compliant.
|
Refer to the Metasys Database Manager Installation Guide (LIT-12011553) . |
|
18. |
If prompted, restart the computer. |
Use the standard procedure to restart the operating system. |
|
19. |
(Optional) If you need the server to be FIPS compliant, enable FIPS mode and install the Metasys FIPS component. |